I'm experiencing inconsistent behaviour with a LM74502H configured as an input surge stopper, with UVLO.
The UVLO/EN pin is connected through a resistor divider to operate falling/rising at 1.14v/1.24v(nom) respectively. The falling edge switch-off behaviour is correct, and predictable, but the device does not reset consistently on the rising edge, sometimes as high as 1.5V
What could be causing this behaviour? I observe the same thing when using the application schematic "9.3 Input Surge Stopper" from the datasheet. The FETs are IPD034N06N3.