Hello,
in our application we use the bq51013b for wireless power to charge a battery and drive a load, max. 300 mA in total. We designed an own PCB RX coil with specs R = 0.8 Ohm and LS = 12 uH. Based on the formulas in the datasheet, the capacitors are around 200nF and 2.1pF. The coil diameter is around 40mm with an inner hole of 15mm. We have a slightly higher distance that specified, around 8 mm.
With this setup, the connection to a standard 15W charger is not stable, but if we double either the inductance or both capacitances the connection becomes stable, either up to 10mm.
How is this behavior explained?
Do we make something wrong during computations?
Thanks four your help