Hello TI,
I am using the slave I2C interface.
I am stuck in the same problem as this thread (which was never answered publicly):
1) How to re-trigger the patch loading?
2) Why is there no reference driver for this? TI should at least have 1 example project on how to do this.
Please post a simple C function (or python or anything) on how to use the patch loader, and how to get it back in patch mode again.
In general I must say that this is probably the worst data-sheet and/or manual I have seen in a long time. The data-sheet and the "Host Interface" manual are full of odd undefined terms and wording, and the example "code in the "Host interface" manual is more or less unusable.
Please help.
Thanks,
/pedro