This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP873220-Q1: How to output default voltage, such as 0.8V

Part Number: LP873220-Q1
Other Parts Discussed in Thread: LP873220

Hi team,

I saw that the LP873220 is an OTP device. So if the customer set BUCKx_EN AND LDOx_EN and BUCKx_EN_PIN_CTRL AND LDOx_EN_PIN_CTRL high level, can they control the output by enable pin when the device power up every time? The output voltage is set as their expectation, such as 0.8V and only if the enable pin set high level, the output will be 0.8V. Is that right? And if  they want to change the output voltage, how to change the voltage?