Other Parts Discussed in Thread: TPS3808E-Q1, TPS3808
Dear Ti,
I want to know that different TPS3808E-Q1 from TPS3870-Q1.
Thank you.
Best Regards,
Inho Jeon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti,
I want to know that different TPS3808E-Q1 from TPS3870-Q1.
Thank you.
Best Regards,
Inho Jeon
Hi Inho,
TPS3808E-Q1 has very low quiescent current typically 0.6μA. It has a high threshold accuracy typically 1% and fixed threshold voltages for standard voltage rails from 0.9 V to 5 V and adjustable voltage down to 0.405 V are available.
TPS3870-Q1 has Low quiescent current 7 µA (Max). It has fixed threshold level 1.5 V, 1.8 V, 2.5 V, 2.8 V, 2.9 V 3.3 V, 5 V.
They both have a CT pin, which it provides factory-programmed and user-programmable reset delay timing options. The reset delay time for TPS3808E-Q1 can be set to 20 ms by disconnecting the CT pin, 300 ms by connecting the CT pin to VDD using a resistor, or can be user-adjusted between 1.25 ms and 10 s by connecting the CT pin to an external capacitor. For TPS3870-Q1 The Capacitor Time (CT) pin is used to select between the two available reset time delays designed into each device and also to adjust the reset time delay by connecting a capacitor.
Depending on the design requirements please find more information on the datasheet.
For TPS3870: https://www.ti.com/product/TPS3870-Q1
For TPS3808: https://www.ti.com/product/TPS3808E-Q1
Best Regards,
Sila Atalar