This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24032A: Can I charge the battery less than 100%?

Part Number: BQ24032A
Other Parts Discussed in Thread: BQ25180

Dear TI experts,

my customer have a question about BQ24032A.

1. Can BQ24032A charge the battery less than 100%, like 80% and terminate charging status?

2. datasheet says that the battery could be recharged if the voltage is under 4.1V, after the charging is complete(4.2V).

Can I change the recharge threshold(4.1V) like 3.9?

Please check this issue. Thanks.

Best regards,

Chase