Other Parts Discussed in Thread: TPS61161
TPS61161
If I need 75mA current for LEDs, What's the external resistor ? Is Rest=200mV/75mA=2.85Ω?
There is a Iout_max in spec. If I need output voltage 25.38V, Is Iout_max =167.5mA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS61161
If I need 75mA current for LEDs, What's the external resistor ? Is Rest=200mV/75mA=2.85Ω?
There is a Iout_max in spec. If I need output voltage 25.38V, Is Iout_max =167.5mA?
Hi Joana,
You can refer to Equation (2) in datasheet to calculate the LED current.
Equation (3) and Equation (4) can help you calculate the theoretical Iout_max.
And may I know what is your end equipment of your application?
BR
Patrick