Hi team,
When tested, the chip's Pin4-tube VSENSE output test was only 0.4V, which according to the manual should normally be at 1.2V. The PIN5 pin ENA hanging VIN has been measured from DC6V-12V, and the output of VSNS has always been significantly low.
When VIN=9V, VSNS voltage is about 0.4V, and when VIN decreases, VSNS will also decrease simultaneously.
The models and values of peripheral devices must be the same as those of reference circuits. Could you help to check the problem of VSNS significantly low? Thanks.