Other Parts Discussed in Thread: LM2767,
We have used the LM2767 on several EVM's and would like to replace it with the LM2765.
The output load is less than 1mA and drives the gates of 3-5 external fets only, and the input slew rate is very slow. We need to generate 9.9V from a 3.3V rail, so we have it configured as a tippler.
Do you see any issue with this change? I understand that the footprint is different and the enable will need to be tied off appropriately.