Other Parts Discussed in Thread: LMR50410
Hello,
I would like to use the LMR51610 in Inverting Buck-Boost configuration, to build a DC/DC converter with the following specs:
- Vin = 24V +/- 10%
- Vout = -15V
- Iout = 0.5A max
This would replace an old design with LM2594HVM-ADJ, in order to reduce size and BOM cost.
My questions are:
- is this possible?
- are there any drawback?
If not possible, I would like to have your suggestion for an alternate in SOT-23 package (I am currently using the LMR50410 converter with success, for a non inverting buck converter).
Thanks, best regards.
Alessio