Hello,
What is the max Iout on the LDO rail if VINLS is less than 3.25V - something like 1.8V?
Thanks In Advance,
John W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the max Iout on the LDO rail if VINLS is less than 3.25V - something like 1.8V?
Thanks In Advance,
John W
Hi John,
For instance, if input is 3.25V and VLDO is configured for 1.8V your max Iout with a 10% tolerance (1.62V at VLDO) is about 100 mA. Reducing input voltage can also increase the amount of current you can pull from VLDO.
What is the
Best Regards,
Juan Ospina