Other Parts Discussed in Thread: TPS3813,
Hey Voltage Supervisor team,
I have a customer using the TPS3813-Q1 for a project and we noticed that there is a discrepancy between the TPS3813 and TPS3813-Q1 datasheets that we're hoping you can help clear up.
In the TPS3813 datasheet there are multiple sections that mention if a GPIO pin is used to drive the WDI input pin then a pulldown resistor must be added to keep the WDI pin from floating during power up. In the TPS3813-Q1 datasheet there is no mention at all of needing a pulldown resistor in any circumstance so can you please help to clarify if there is indeed a functional difference between these two devices which warrants not putting the pulldown for the -Q1 version?
Also, what happens if the WDI pin is left floating for a period of time?
Best regards,
Matt Calvo