Other Parts Discussed in Thread: TPS389006
Hello.
Is there a more detailed description on how the TPS389006 decide on which I2C it has? Currently there is a small table in the datasheet, but don't really explain it any further. This question accurs, because the majority of the values are not that common and would need an extra feeder especially for this IC. So the idea is just to use more frequent one. For example a 47k for a 47.5k (which should be fine, as even a 1% tolerance is in that scope).
So my questions would be here:
- How high can be the tolarance of the resistors?
- Which range of resistors are still usable to select the respective I2C address?
- Which voltage range is needed for the the respective I2C address (Currently I assume that the voltage drop is measured with the 20uA current)?
Kind regards.