This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28251: Output ripple is too large as 500mV

Part Number: UCC28251
Other Parts Discussed in Thread: UCC28250EVM-501, UCC28250,

Hi team,

I tested UCC28250EVM-501. Input 40V, output 3.3V, load is 10A. And I found that the ripple can reach to 500mV.  And I found that the ripple is affected by the switching node. Could you pls help with this issue? I have used a short GND to probe.

Thanks!

Rayna