Hi Team,
Do we have voltage monitor solution can achieve below waveform? Thank you.
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
You can use the TPS3840PL33DBVR which has a 3.3 V threshold and an adjustable delay time. Per your scope shot specs, you can add a 5.6 uF cap on the CT pin of the IC to achieve a 3-4 s delay. Make sure to also add a ceramic cap with a 1 uF on VDD as a bypass capacitor to ensure that the device can still power up correctly in noisy applications.
Please let me know if you have any other questions,
Joshua Austria