Other Parts Discussed in Thread: BQ25180, BQ25155
Hello,
We use BQ24031 battery charger. Can I get a low battery indication using the charger itself or do I need additional voltage monitoring IC?
Thanks in advance and BR
Joel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Joel,
As the BQ24031 is standalone, it's more restricted in what it can show and so there's no low battery indication. You're correct in that you'll need a voltage monitoring IC.
If you're able to, the BQ25155 has a built-in ADC that can provide the battery voltage measurement. It is only max 500 mA so if that might be a problem, you can look into the BQ25180 which can provide a battery undervoltage lockout (BUVLO) threshold that can act as a low battery indicator.