Hello,
I'm testing a custom board with BQ25175YBGR on it and a 4.35 li-ion cell with a capacity of 545mAh. The PCB has Riset at 750 Ohms, which would indicate a charge rate of 400 mA. Measuring with a multi meter, the battery voltage is 3.4v, yet only approximately 100 mA flows into the battery when measuring.
Looking at the DS I would assume pre-charge is ended when the voltage reaches above Vbat_low but this never happens, at least for 10 minutes, when I decided to stop testing.
Any advice?