This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8D6C24: TPSM8D6C24MOWR - VSEL calculation

Part Number: TPSM8D6C24

Hi

I need to get 0.95V in the Vout, I try to understand the calculation 

according to table 7-12:

Resistor divider code = 2

Code = (0.95-0.9)/0.01 = 5

So in this case, I need 2 resistors from Vsel Pull up to BP1V5 and Pull down to AGND

Vsel to AGND (Rbot) = 12.1K and Pull up to BP1V5 = 30.1K

Am I right?

One more question - I seen in the Evaluation that AGND not connected to PGND. But in the datasheet recommendation is to connect the AGND direct to the E pad. that mean the connection is inside the chip?

Thanks