Hi,
In the guidebook, the waveform of hiccup mode is shown. In the hiccup mode, 64 cycles current limits are detected, the switching is stopped and restart after 32768 cycles. As the frequency is 250kHz, this time of detection should be 0.265ms. But in the guidebook, the time that I(o1) is at high level seems too large.
I also test the EVM. The waveform is shown as follow. The time of HICCUP is larger than the results in guidebook.