Other Parts Discussed in Thread: TPS7A24
Hi
Could you help to suggest products that can replace G2920-T11U(have ADJSet to 5.33V Output), need P2P
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gareth,
TLV709 does not have an EN option. If the customer doesn't need 35V then TPS7A24 could work here.
TLV709 | TPS7A24 | |
Iout(Max)(A) | 0.15 | 0.2 |
Vin(Max)(V) | 30 | 18 |
Vin(Min)(V) | 2.5 | 2.4 |
Vout(Max)(V) | 28 | 17.75 |
Vout(Min)(V) | 1.2 | 1.24 |
Fixed output options(V) | 3.3, 5 | 1.25, 1.8, 2.5, 3, 3.3, 3.6, 5 |
PSRR @ 100 KHz(dB) |
60 | 22 |
Noise(uVrms) | 425 | 300 |
Accuracy(%) | 2 | 2 |
Dropout voltage (Vdo)(Typ)(mV) |
400 | 160 |
Iq(Typ) (mA) |
0.003 | 0.002 |
Output capacitor type | Ceramic | Ceramic |
Thermal resistance θJA(°C/W) |
131.7 | 167.8 |
Operating temperature range(C) |
-40 to 125 | -40 to 125 |
Package size: mm2 | 18.4275 mm2: 4.5 x 4.095 (SOT-89|3) | 5 mm2: 1.6 x 2.9 (SOT-23|5) |
Packages | SOT-89|3 |
SOT-23|5 |
Thanks,
Prakash L