Other Parts Discussed in Thread: NE555
Hi. In DS I found only on-resistance for PWRGD with 50R (typ) if active. But due to open drain output I guess there is still a min voltage level on output if PWRGD asserts to low.
My application runs with 24V Vin, 5V Vout, ca 100mA out, -25...+85°C. PWRGD will connect to NE555 timer on Reset pin that needs <= 0.3V to activate Reset in worst-case szenario.
Does anyone knows if I can use only 50R on PWRGD output to calculate level or are there any other limitations?
Thx & KR Tom