Hi
The customer design with BQ28Z610-R1, when do the short test the MOS was burn.
1. Cell capacity 11000mAh, total voltage 8.9V
2. MOS model: AOC3870C * 4
Please help check the schematic.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The customer design with BQ28Z610-R1, when do the short test the MOS was burn.
1. Cell capacity 11000mAh, total voltage 8.9V
2. MOS model: AOC3870C * 4
Please help check the schematic.
Thanks
Star
Hello Star,
There could be many causes of electronics failures, but for a short circuit in a battery the following are some possible causes to consider and test:
Please reference to this FAQ for SCD debugging. How to debug FET failure resulting from short-circuit testing
I am inclined to say this behavior is due to bullet point number 4 above. The gate of each FET requires a small gate resistance to avoid oscillations. Please also reference to this app note - Tips for Successfully Paralleling Power MOSFETs
Regards,
Jose Couso