This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR54406: Can't get the specified current value with LMR54406

Part Number: LMR54406
Other Parts Discussed in Thread: LMR54410, TPS628510, TPS62824, TPS628511, STRIKE

We purchased the LMR54406FDBVR and set it to generate 2.5V from the input voltage of 5V, referring to the application note on p.18 of the data sheet. Resistance values 47k and 22.1k. L=10 μH. Output stage capacitor 22μF.


We were able to obtain a voltage of around 2.5V, but the current was only a few mA. (If lower the resistance value with a variable resistor, the output voltage will drop to 0V when only a few mA flow.)
There is no problem because the 5V power supply that is supplied is capable of flowing up to 5A.

P.S.

Test is on a breadboard.
The peripheral passive components used are discrete products.

Thank you for your advice on possible causes.

Best regards,

Masaki Noguchi 

NEMOTO & Co.,Ltd