Other Parts Discussed in Thread: UCC21530, , UCC14141EVM-068
My gate driver is UCC21530
My high side MOSFET is Infineon_IPTC044N15NM5
Switching frequency working at 100KHz.
The duty cycle can be adjusted from 0% to 60%.
The voltage of the DC bus is 80Vdc.
Can anyone give an example of calculating RLIM based on my situation above?
In datasheet, Equation 9,
Rlim = Vout2 / Ivout2_max - Rlim_int
How to select Ivout2_max??