Other Parts Discussed in Thread: LM5088
I'm using BQ24075 as a charger in my board. Conditions:
Input voltage (VIN) is at minimum (4.38V).
EN1=LOW, EN2=HIGH, using Ilim=1.5A (1.1K) and Iset=1.4A (620R)
CE = GND and SYSOFF = GND
No load at OUT, and voltage measured at this point is 4.25V
With battery connected charge current is only 200mA (0.42V) (measured at Iset pin using this equation VISET = ICHARGE / 400 × RISET). If I turns cjharge on without battery connected I expect CHG pin to be high-Z, but it blinks. With battery connected CHG goes LOW and led turns on, but only with 200mA.
Questions, with EN1, EN2 configured to use Ilim and Iset, why the output current is too low? Vin is at minimum but inside the operational range and I have no load at OUT.
For reference battery voltage at this situation is 3.6V.