Other Parts Discussed in Thread: BQ40Z60
Hello,
I am currently working designing a BMS using a BQ40z80. OCD is set to 5A. I am using a power supply in-place of a cell stack and a programmable load.
Everything works and trips as expected at slightly above 5A.
Increasing the load current to 10A or above causes the DSG output to transition from 27Vdc to 0V as expected, but will then come back at whatever the input voltage is.
The BMS no longer will control the DSG output.
I have attached my schematic to see if I have made any design mistakes.
So far I have lowered R10 to 4.7k and 2.2k with different results. DSG will go to 20Vdc for a few more cycles and then fail.
I have changed the discharge FET count from 4 to 2 with no change.
Any help is appreciated
.