Other Parts Discussed in Thread: TPS61022, TPS61022EVM-034
Hi.
Looking at the datasheet 1PAGE, VIN=0.5V ~ 5.5V.
6PAGE FIGURE 6-3, which indicates that the output power current can be 1A or higher when VIN = 1.8V - 4.2V.
What is IOUT when VIN=0.5V ~ 1.7V?
I'm going to use 5V/0.8A with AA battery 1EA and BOOSTER. Do you have any recommendations?
Best regard,
KWON.