Other Parts Discussed in Thread: LM2611, , LM2776, LM2775
Dear,
I bought the EV of the LM2611 device. I tested the performances: Vin = 5V
- Without loads (Iout = 0 mA), the convertor is operationnal
- If the output current is growing above 8 mA, the EVAL board do not operate correctly. We do not obtain the correct value. We have an issue due to oscillation. The board is loaded by an ideal resistor.
Wer do not understand the origin of this issue. Please, could you help us ?
Thank you in advance.
Best regards!