Hello,
We are using the LM25118 in a design. We had an issue with some devices where the 24V VIN voltage was directly applied to the UVLO pin. This is over the absolute maximum rating of the UVLO pin, which is 16V. The LM25118 still works as it outputs the correct voltage. For the UVLO pin, we have to run some tests to determine if it still functions as expected.
Do you think this can cause long term issues for the LM25118 IC? If we determine that the UVLO function still works, are there other potential issues that we should be aware of?
Thank you