Hi
The design is DC/DC from input 5.5V and output 0.95V , Current 46A. A and B connected tougher
I need help in Design review and need layout support
Please attach file my design and please review and comments
As I understand that AGND and PGND are connected inside the component so I don't need to connect them externally in one point
from datasheet section 10.1 Layout Guidelines : "Those components can be terminated to AGND with a minimum return loop or bypassed to the copper area of a separate low-impedance analog ground (AGND) that is isolated from fast switching voltages and current paths and has single connection to PGND on the thermal pad through the AGND pin"
Because I using with the two parts of the DC/DC (to get 46A) I need to connect the AGND_A and AGND_B together, So what is the best way to short them to get minimum return loop and to be isolated from fast switching?.
Thanks