Hi All
please help me to understand this completely, I just want to make sure.
The maximum dimming ratio for this LED driver is 32000:1, using 152 Hz
I want to know if my understanding is correct. (please correct me if i m wrong)
so the maximum ratio is 32000:1. Is it true that no matter what PWM frequency we choose, the maximum dimming ratio for each PWM frequency remains the same 32000?
And for this sentence "Dimming ratio 32000:1, using 152 Hz"
is this definition correct?
32000 : Maximum Brightness
1 : Minimum Brightness
Using 152 Hz Frequency : can be adjusted or dimmed at very fast rate 152 times/second
Thank youu