This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A92: tps7a92

Part Number: TPS7A92

Hi, 

I'm planning to use TPS7A92 for my project, 

this is my requirement,

Vin=5V

Vout = 3.8V

Iout = 1.6A

Ta= 70C

based on datasheet, i have done some calculations,

part has RθJA = 56.9 °C/W, if we calculate the Pd(max) of this part,

 

Pd(max) = Tj(max)-Ta)/ RθJA

                =  (125-70)/56.9

                = 0.966W

As per our requirements, Power dissipation will be,

 

Pd = (Vout-Vin)*Iout

      = (5-3.8)*1.6

      = 1.92W

is my calculations are proper? With the calculation i have conculded that i cant use this part. 

Do you have any suggested part?  

Regards,

Hareesh