Hi,
For the circuit similar to the one mentioned in the datasheet of TPS563257, I have connected 100k( to +Vcc) and 32k (to -Vcc) resistors instead (10nF is not connected) for the voltage divider to the enable pin.
The supply voltage is steady 5V DC, the voltage divider is supposed to deliver 1.49V to the enable pin (which is delivering 1.170V mostly due to the change in resistor values I reckon), inductor value was suggested to be 680nH which has been used in the circuit,
but it only delivers 0.78V instead of the required 0.85V.,
What could be the possibility of the 0.7V drop?
Please consider Figure 8-1 from datasheet of TPS563257DRLR
s/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/4452.tps.png