I was designing and evaluating it, but the following symptoms occurred.
Design specification:
VIN=14V,Vout=10V
f=100kHz, Iout=3.5A
1. Voltage does not come out correctly when there is no load.
2. When the motor was connected and a load was applied to the motor, and the load current went from about 1A to 2A, something like a ripple was seen in the output waveform, which was higher than the normal voltage.
I had put a 9.1Ω resistor in the gate of the MOSFET (IRFH5300), but when I shorted it, "1" improved.
It seemed to be related to MOSFET.
So my question is,
1.Has the maximum operating capacity of the external MOSFET been determined?
If it is determined, how can I find it from the data sheet?
2.Isn't it usually used to put a resistor in the gate?
However, this seems to exceed the output current capacity of the gate driver on the power supply IC side.
3.Are Forced HO off-time and Minimum HO on-time of PWM COMPARATORS the same even if the Frequency of Operation changes?
Also, does this mean that I have to use a MOSFET that can be turned on with Minimum HO on-time (100ns) and a MOSFET that can be turned off with Forced HO off-time?