Other Parts Discussed in Thread: , TPS3760
Hi,
I hope you will be able to help me with this problem:
Description:
- I am having issues with the TLV803S. I am using it to monitor the voltage of a Li-Ion battery and shut the output down if it falls below the threshold.
Problem:
- The /RESET output pin is always low. I have measured the voltage between GND and VDD as 4V. This should make the /RESET pin go high due to the pullup resistor. It remains low.
Tests:
- I have bridged Q5 just in case it was a GND problem. The switch SW1 is definitely open.
- +BATT does output power from the battery when I remove the TLV803S from the circuit - so it is the culprit.
- I have tried a TLV803R instead and it does work if I poke with my finger (some coupling? - all the solder joints are solid), but once the voltage falls below the threshold, even if it increases again the /RESET pin stays low (and never goes high again). It seems to have some sort of latching behaviour.
- I have tried reducing R98 from 430k to 100k - it made no difference.
- I have tried another TLV803S in case the first one was damaged - it made no difference.
I am growing a bit suspicious about the spec as well. The new TLV803E which is the new generation has an interesting first line in the datasheet:
Ensured? Isn't it ensured in the TLV803S?
Kind Regards