This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51430EVM: Output Ripple

Part Number: LMR51430EVM
Other Parts Discussed in Thread: LMR51430

There are two questions about this EVM.

1. Why both C8 and C9 are not placed on the EVM as below diagram? on the EVM bom, it looks both has placed. 

2. Customer tried to test EVM without any component modified. the Vpk-pk is very high. Could you guide how to improve it efficient? thanks. 

 

Dynamic Load Condition:

On time: 10mS

Off time: 5mS

S/R: 6A/uS

Test 1: 0.3A -> 2.5A, Vpk-pk : 807mV

Test 2: 0.3A -> 3.0A, Vpk-pk : 1.07V (waveform is as below)

Here are more waveforms tested.

LMR51430EVM Test Waveform.zip