This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064RNQEVM: original Project file (.pjt) and Binary file (.bin) about TPS65982

Part Number: TUSB1064RNQEVM
Other Parts Discussed in Thread: TUSB1046EVM, TPS65982, TUSB1064, TUSB1146, TPS65987, TUSB1146EVM

Hi team,

I am hoping to get the original Project file (.pjt) and Binary file (.bin) that comes standard on the TPS65982 chip, that is on the TUSB1046EVM evaluation board.

Thank you!I would greatly appreciate it!

  • Shawn:

        Sent TUSB1064 project file, what customer  do you support?

    Regards

    Brian

  • Brian:

    OK,Thanks a lot,my customer is  BYD and Volvo,i need to design a machine to test car charger, as you know,many cars has dp function via Typec.

    Thank you again for your timely reply!

    Best Regards

  • Brian:

    Could you also  send me the original Project file (.pjt) and Binary file (.bin)  on the TUSB1046EVM evaluation board?

    i need to design PCB Board about DP Source and DP Sink.So i need both of the two Project files(TUSB1046EVM and TUSB1064EVM).

    It's really troublesome of you.

    Bsst Regards

    Shawn

  • Shawn:

       You need TUSB1146 or TUSB1046 project file? I just sent TUSB1146 file.

    Regards

    Brian

  • Brian:

    Yes, I need Both of them.i check the file you sent, is it a drc format file?Actually,as some others have asked before, I also need the project files to customize some settings of the PD-Controller on the TUSB1046EVM and TUSB1064RNQ EVM. I need to use the “Application Customization Tool” to debug PD-Controller.

    Regards

    Shawn

  • Brain:

    I also saw that someone in the forum raised the same question and the response from the forum manager.

    And I already noticed that PS65982 is NRND (Not Recommended for New Design) , and I will  also use the TPS65987 in new designs.But for now I have the TUSB1046 EVM board and TUSB1064EVM board ,both of them are equipped with the TPS65982, and in order to continue my test I need at least to know what the current settings for the chip on this board are. Cause im studying how to set PD Controller.I am a bit anxious about this project, so thank you for your timely response

    Regards

     Shawn

  • Shawn:

            I sent PD configuration tool to you as well.

            You can start with TUSB1146EVM and TUSB1064EVM, TUSB1046 is old device and performance is not good as TUSB1146.

    Regards

    Brian