This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: At what current does the frequency drop from 2 MHz?

Part Number: LM27761

The datasheet for the LM27761 states that the switching frequency can drop from 2 MHz if the current draw on the output is low. The datasheet states that the switching frequency could drop as low as 2 kHz if the current draw is low enough.

I'm considering this part for a sensitive analog system, so I need to ensure that the ripple frequency is sufficiently high so that it can be rejected by my signal chain.

I couldn't find any information about what the current draw amount where the switching frequency starts to drop from 2 Mhz. I expect my system to pull about 15 mA.