This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62903-Q1: Need small size inductor with TPS62903-Q1

Part Number: TPS62903-Q1

Hi Team,

My customer need small size solution because of Camera module application.

is it possible to use small size chip inductor with below condition? 

I know that we have other solution but Customer need to make sure about inductor size with TPS62903-Q1.

Input : 3.8V output: 0.8V@3A.  

current Webench result is Coilcraft XFL4020-102MEB (L = 1 µH, DCR = 10.8 mΩ, IDC = 5.4 A )

Best regards

Joey Kim