Hi TI Team,
Can you help me to look at the application schematic diagram of LM5176 and give me some suggestion?
Usage: LM5176 6-38 V buck-boost 12V, the range of input source is from 6V to 38V, I want to use LM5176 to buck-boost and keep the stable output at 12V/10A.
Objective: To maintain a stable output at 12V all the time, that is, when the input power is 6V, the output needs to be boosted to 12V, and when the input power is 38V, the output needs to be stepped down to 12V.
Thanks