Hello,
Is there an additional current consumption of the eFuse when the input voltage is between the 5.4V and 7.6V ?
The datasheet only shows the current when the input is at its absolute maximum value of 20V, with the over voltage protection already enabled.
Also, Is there a graph of Iin(on) versus RLIM ?
Thanks,
Yassine