This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25200: Over-Voltage Clamp Current

Part Number: TPS25200

Hello,

Is there an additional current consumption of the eFuse when the input voltage is between the 5.4V and 7.6V ?

The datasheet only shows the current when the input is at its absolute maximum value of 20V, with the over voltage protection already enabled.

Also, Is there a graph of Iin(on) versus RLIM ?

Thanks,

Yassine

  • Hi Yassine,

    Thanks for reaching out.  All the test conditions we are testing in final test are mentioned in datasheet. We would not have data apart from that. 

    Iin(on) is not supposed to change with RILIM. 

     Regards

    Kunal Goel