Hello
I'm using BQ24123 charger on 2Cell battery (8.4V)
while battery is in cutoff - it start the charging.
here is my circuit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff
I run the test:
Battery connected
No input power: Vbat = 0V Ibat = 0A State1 = 0 State2 = 0
input connected: Vbat =6.3V Ibat = 0A State1 = 0 State2 = 0
So i understated that there is Error state and no charging? correct?
Hi Uri,
If the battery is connected but no voltage at BAT pin, then the battery protector pack protector has tripped due to overvoltage, overcurrent, or undervoltage. What is the input voltage applied? Is /PG low? Is Vref=3.3V? When you say Statex=0, I assume you mean both are low=gnd? It so that isn't a valid state combo. What is the voltage on TS pin?
Regards,
Jeff