Other Parts Discussed in Thread: BQSTUDIO, BQ35100
Dear all,
I am using BQ35100EVM-795 EvalBoard in order to characterize the current absorptions of a PCB board supplied by a Li-SOCl2 battery by using BQSTUDIO.
The current range is 20uA - 40mA, so I decided to solder a 3.3 Ohm resistance as sense resistor on the EvalBoard.
As a matter of fact, in this way I could measure from 2.3uA ( = 0.125 V/ 3.3R /(2^14-1) ) up to 37.8mA ( = 0.125V/3.3R).
After having calibrated the fuel gauge, I decided to test his accuracy before use it on my board.
However, I noted that:
1. The minimum measured current is 1mA. With currents lower than 1mA, it measures 0mA
2. The current offset error is too high (it counts 2uAh every minute at no load condition, that is more or less 100uA of offset current), even if the calibration procedure was OK. How can I minimize this error?
Looking forward to hearing from you soon.
Kind regards,
Vladimir Zitoli