Other Parts Discussed in Thread: LM3488, LM5155, LM5157
Dear TI support,
I would like to ask you about the LM3488 in Sepic configuration:
Vin = 6V to 18V
Vout=13.5V
Iout_max = 0.9A
fsw = 220kHz
L = 15uH
Cout = 100uF
Feedback loop bandwidth = 12kHz
By running an automated measurement setup (Vin and Iout parameters are swept), the below results are generated:
This is a very slow measurement (Vin is set, 1 sec waiting time, Iout is set, 1 sec waiting time, Vout read).
My question is regarding the output voltage elevation at no-load/minimum load:
1) could you please confirm this is a normal behavior of this IC?
2) is this coming from the Vcomp behavior? (snippet from datasheet)
Thanks in advance,
Kind regards,
Csongor