This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9081: Upper bound on flash write time?

Part Number: UCD9081
Other Parts Discussed in Thread: UCD9090

Hi experts

I have a question on UCD9081 and UCD9090.

What is the maximum Flash write duration expected for the part? Is it possible to put an upper bound on the time it takes to write the flash, and where the part is consuming slightly higher power than normal operation?

Thanks!

Jim B

  • Hi

    the information for UCD9090 has been explained in the other thread.

    For the UCD9081, the typical time to program one word is 35 clock flash timing generator frequency(range from 257KHz to 476KHz).

    As said it is max 7mA.

    Regards

    Yihe