I have some queries related to the design of the BQ24171 charger circuit.
Q1. In the application circuit of the same, a N channel reverse blocking FET is added in the circuit ,whose source pin is connected to the source of ACFET. how it blocks the reverse polarity? since the drive voltage for the both FET's are considered as CMSRC +6V . it will be completely on unless a low drive signal is provided to the gate.so could you please explain how it act as RBFET?
Q2. what is the purpose of ACDRV ?