Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hi,
I`m trying to start working with the battery fuel gauge and I have some questions:
this is my hardware and I'm connected to the device via EV2400:
1. I can't get accurate current readings from bqstudio, I'm drawing 2000ma with a constant load, and in the bqstudio I'm reading -1452mA.
at the calibration screen, I only have voltage calibration.
2. I'm trying to perform a relax-discharge-relax test but after discharge, I get power loss (battery cut off) and can't read from the IC.
how the test can be done if I need to discharge the battery and still get communication with the device?
my final goal is to make a golden file for my battery with the IC.
best regards,
Kfir Maymon.