Other Parts Discussed in Thread: LM5170, PMP21943
Hi,
I want to add external Gate driver to LM5170 in order to implement buck converter with:
- Input voltage 40VDC t0 250VDC.
- Output voltage 31VDC.
- Output power 1500watt.
- High efficency 99%.
How i connect the external gate driver to LM5170?
PLS advise MOSFET.
Do i have to add isolation between input and output when input is alternator in delta connection?
PLS explain.