Hi Experts,
LM5163-Q1 is under evaluation on customer side. The max output current is 28mA, the minimum output current is 3mA. Customer is worry about the ripple voltage when the device enter sleep mode.
Could you share the ripple test result when LM5163-Q1 enter sleep mode? Thanks.
Here is the schematic information from customer:
- Ron=100k
- L=68uH
- Output Capacitor: 4.7uF
- Input Voltage: 18-60V
- Output Voltage: 9V
- Output Current: 3~28mA
Best Regards
Songzhen Guo